2023-08-18 5:24 AM
Hi everyone, I am a bit confused about this.
In STM32CubeMX tool, I configured SDRAM 100MHz, the tool GUI shows result 100MHz as well, then I generate code then test.
I check SD clock pin, it is 10ns on each single clock, no matter the clock is high or low, seems I config it correctly.
But if we say frequency is one lock high and one clock low (or same as PWM), mean currently SDRam runnng only 50MHz (one high + one low = 10 + 10 = 20ns => 50MHz).
So, in STM32H743 datasheet says maximum SDRAM 100MHz, is this 100MHz only one clock 10ns, no matter high or low, or this is a combination of one high and one low (5ns each clock)?
Many thanks,
2023-08-18 11:33 AM
Perhaps diagram what you are seeing, specifically, and with respect to other address, data or control signals.
I'd expect a 50/50 duty cycle with a period of 10 ns, with sufficiently aggressive edges.
The timing units of other signals should be in multiples of 10ns, ie relationships for RAS / CAS etc, and most memories furnishing responses with 6-7 ns
The burst data transfer rate should be measurable. SDRAM has a relatively large amount of overhead in small random transactions.
2023-08-19 8:06 AM
"...I'd expect a 50/50 duty cycle with a period of 10 ns, with sufficiently aggressive edges..."
Can I understand SDRAM 100MHz should be mean 5ns + 5ns low = 10ns total?
Because 20ns seem to be very slow as I see.
2023-08-19 10:24 AM
Would suggest code that unpacks RCC clocks, SYSCLK, AHB, APB and PLLs and then to the FMC/SDRAM settings. Review the clock chain.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.