2023-04-14 11:28 PM
i am using one side microcontroller stm32103 which have can1 protocole does this work with othere microcontoller stm32g0b1re which have FDCAN protocol.?
does both communicate with each other ?will read and write the data?
Solved! Go to Solution.
2023-04-15 7:33 AM
Dear @Ranjeet Singh ,
Yes, this is possible FD-CAN is compatible with CAN2.0 and you can enable STM32G0 to work in CAN2.0 legacy mode. For more details on STM32 CAN and FD-CAN implementations and Differences see this Application Note : AN5348
Introduction to FDCAN peripherals for STM32 product classes - Application note
Cheers
2023-04-15 7:33 AM
Dear @Ranjeet Singh ,
Yes, this is possible FD-CAN is compatible with CAN2.0 and you can enable STM32G0 to work in CAN2.0 legacy mode. For more details on STM32 CAN and FD-CAN implementations and Differences see this Application Note : AN5348
Introduction to FDCAN peripherals for STM32 product classes - Application note
Cheers
2023-04-15 8:17 AM
All FD-CAN and XD-CAN devices have a compatibility mode, and interoperate with standard CAN devices.
Except for some niches, market penetration of these new highspeed CAN standard is not very high.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.