2024-05-25 5:14 AM
I am trying to implement usart2 tx with dma1 stream 6 channel 4. I have tested the usart2 tx independently and it worked perfectly, but the dma part was not that lucky, it just wasn't send anything and I couldn't find anything wrong in my code. Appreciate for any help.S here's my code:
void RCC_SetUp(){
RCC->APB1ENR |= (0x1<<0);//TIMER2 enable (84MHz)
RCC->AHB1ENR |= (0x1<<0);//A
RCC->APB1ENR |= (0x1<<17);//USART2 enable
RCC->AHB1ENR |= (0x1<<21);//DMA1 enable
}
void GPIO_SetUp(){
GPIOD->MODER |= (0x1<<26);
GPIOD->MODER &= ~(0x1<<27);
//PA2 alternate function
GPIOA->MODER &= ~(0x01<<4);
GPIOA->MODER |= (0x01<<5);
//PA2 Tx
GPIOA->AFR[0] |= (0x01<<8);
GPIOA->AFR[0] |= (0x01<<9);
GPIOA->AFR[0] |= (0x01<<10);
GPIOA->AFR[0] &= ~(0x01<<11);
}
void DMA1_Stream6_IRQHandler(void)
{
if(DMA1->HISR & (0x1<<21))
{
DMA1->HIFCR |= (0x1<<21);
}
}
volatile uint8_t buffer[] = "USART2_TEST\r\n";
void DMA1_SetUp()
{
//make sure dma is off
DMA1_Stream6->CR = 0;
while(DMA1_Stream6->CR & (0x1<<0))
{
//wait for DMA to disable completely
}
//channel 4 selected
DMA1_Stream6->CR |= (0x1<<25);
DMA1_Stream6->CR |= (0x1<<26);
DMA1_Stream6->CR |= (0x1<<27);
//DMA transfer complete interrupt
DMA1_Stream6->CR |= (0x1<<4);
//Memory increment
DMA1_Stream6->CR |= (0x1<<10);
//Circulation enable
// DMA1_Stream6->CR |= (0x1<<8);
//Medium Priority
DMA1_Stream6->CR |= (0x1<<16);
//memory to peripheral
DMA1_Stream6->CR |= (0x1<<6);
//src mem address
DMA1_Stream6->M0AR = (uint32_t)buffer;
//dst periph address
DMA1_Stream6->PAR = (uint32_t)&(USART2->DR);
//number of item for dma2
DMA1_Stream6->NDTR = sizeof(buffer);
//setup NVIC
NVIC->ISER[2] |= (0x1<<6);
//enable DMA
DMA1_Stream6->CR |= (0x1<<0);
}
void USART2_SetUp(void)
{
USART2->CR3 |= (0x1<<7);//DMA transmit enable
USART2->CR1 |= (0x1<<9);
//BR = 115200
USART2->BRR = (22<<4);
USART2->BRR |= 13;
USART2->CR1 |= (0x1<<3);//Tx enable
USART2->CR1 |= (0x1<<13);//Usart2 enable
USART2->SR &= ~(0x1<<6);//clear tc bit
}
int main(void)
{
Clock_SetUp();
RCC_SetUp();
GPIO_SetUp();
USART2_SetUp();
DMA1_SetUp();
while(1)
{
}
}
2024-05-25 8:27 AM
First of all, welcome to the community. I skimmed through your code and gotta say its was pretty clean. All are correct, except the lines:
//channel 4 selected DMA1_Stream6->CR |= (0x1<<25); DMA1_Stream6->CR |= (0x1<<26); DMA1_Stream6->CR |= (0x1<<27);
bit 25 and 26 should be 0 right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.