2015-03-10 2:16 PM
Hi,
I'm using ADC and DMA. For learning purposes no interrupts, just polling LIFR. Staring conversion with ADC_CR2_SWSTART. As soon as TCIF is set, I'm writing 1 to ALL flags to LIFCR (LIFR becomes 0) then re-enabling DMA. Do ADC_CR2_SWSTART again and no more flags in LIFR...EOC flag for ADC is set.Why is that? What am I missing? #dma2015-03-10 3:52 PM
I don't know ( I never used DMA with ADC), but maybe you might want to try to play with something like a simple timer (*not* the advanced like TIM1/TIM8) or USART. ADC might have its own issues, and/or the bits enabling DMA in the ADC.
Also, look at the DMA registers after the ''restart'', post them here if you want. JW2015-03-10 5:43 PM
All DMA registers are the same as they were before the first time i.e after init().
DMA after init() first successful Before the next transfer transferLISR 0 0x00000C00 0 HISR 0 0 0S1CR 0x04002C01 0x04002C00 0x04002C01
S1NDTR 0x4 0 0x04S1PAR 0x4001224C 0x4001224C 0x4001224CS1M0AR 0x20000000 0x20000000 0x20000000S1FCR 0x00000020 0x00000020 0x00000020ADC3 DMA is looping SR 0 0x00000010 0x00000012CR1 0x03000100 0x03000100 0x03000100 CR2 0x00000101 0x00000101 0x000001012015-03-11 1:11 AM
Nice catch, Baruch!
Indeed, the text in ADC chapter contains this:No new DMA request is issued to the DMA controller if the DDS bit is cleared to 0 in the
ADC_CR2 register (this avoids generating an overrun error). However the DMA bit is
not cleared by hardware. It must be written to 0, then to 1 to start a new transfer.
A hidden bit influencing hardware's behaviour is an, ehm, really bad idea, if you ask me... Thanks for sharing this info. JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.