2016-12-20 5:12 PM
Hi again,
I am trying to use DMA now as its more straightforward but still not working for me. Ain[0] below is only reading some weird voltage 0-0.17V instead of 1.3V and Ain[1] reads nothing stays 0. can you please have a look and let me know what might have gone wrong:
#include 'stm32f7xx_hal.h'#include 'global.h'#define NO_OF_CHANNELS 2#define NO_OF_ADCs 1//Note that Interrupts for all peripherals are located in the xxx_msp file and xxx_it
void MX_ADC1_Init(void);void MX_DMA_Init(void);void readAins(void);void MX_DMA_Init(void)
{/* DMA controller clock enable */__HAL_RCC_DMA2_CLK_ENABLE();/* DMA interrupt init */
/* DMA2_Stream0_IRQn interrupt configuration */HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);}
void MX_ADC1_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/hadc1.Instance = ADC1;hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;hadc1.Init.Resolution = ADC_RESOLUTION_12B;hadc1.Init.ScanConvMode = ENABLE;hadc1.Init.ContinuousConvMode = DISABLE;hadc1.Init.DiscontinuousConvMode = DISABLE;hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;hadc1.Init.NbrOfConversion = 2;hadc1.Init.DMAContinuousRequests = ENABLE;hadc1.Init.EOCSelection = DISABLE;HAL_ADC_Init(&hadc1);// if (HAL_ADC_Init(&hadc1) != HAL_OK)// {// Error_Handler();// }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/sConfig.Channel = ADC_CHANNEL_2;sConfig.Rank = 2;sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;HAL_ADC_ConfigChannel(&hadc1, &sConfig);if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{Error_Handler();}sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;HAL_ADC_ConfigChannel(&hadc1, &sConfig);if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){Error_Handler();}// All Channels has to be preconfgured here as above}void readAins(void){
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&value2, 2);Ain[0]=value2[0];Ain[1]=value2[1];}msp file:
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hadc->Instance==ADC1){/* USER CODE BEGIN ADC1_MspInit 0 *//* USER CODE END ADC1_MspInit 0 */
/* Peripheral clock enable */__HAL_RCC_ADC1_CLK_ENABLE();/**ADC1 GPIO Configuration
PA0/WKUP ------> ADC1_IN0PA1 ------> ADC1_IN1 */GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2;GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;GPIO_InitStruct.Pull = GPIO_NOPULL;HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* USER CODE BEGIN ADC1_MspInit 1 */
/* USER CODE END ADC1_MspInit 1 */
/* Peripheral DMA init*/hdma_adc1.Instance = DMA2_Stream0;
hdma_adc1.Init.Channel = DMA_CHANNEL_0;hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;hdma_adc1.Init.Mode = DMA_CIRCULAR;hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH;hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE;hdma_adc1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL;hdma_adc1.Init.MemBurst = DMA_MBURST_SINGLE;hdma_adc1.Init.PeriphBurst = DMA_PBURST_SINGLE;HAL_DMA_Init(&hdma_adc1);// if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)// {// Error_Handler();// }__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);}
}
void HAL_ADC_MspDeInit(ADC_HandleTypeDef* hadc)
{if(hadc->Instance==ADC1)
{/* USER CODE BEGIN ADC1_MspDeInit 0 *//* USER CODE END ADC1_MspDeInit 0 */
/* Peripheral clock disable */__HAL_RCC_ADC1_CLK_DISABLE();/**ADC1 GPIO Configuration
PA0/WKUP ------> ADC1_IN0PA1 ------> ADC1_IN1 */HAL_GPIO_DeInit(GPIOA, GPIO_PIN_0|GPIO_PIN_1);/* Peripheral DMA DeInit*/
HAL_DMA_DeInit(hadc->DMA_Handle);// __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);}/* USER CODE BEGIN ADC1_MspDeInit 1 *//* USER CODE END ADC1_MspDeInit 1 */
}
2016-12-21 11:02 AM
Hi
Alzqhoul.Esam
I have moved your post to
https://community.st.com/community/stm32-community/stm32-forum/activity
where product-related questions are asked. If you have any further questions post them here.Thanks
Oli
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.