2016-12-15 7:50 AM
What is the purpose of GRP{x} in LL_{BUS}_GRP{x}_EnableClock() in CubeF0?
Where is it documented?
Thanks,
JW
Solved! Go to Solution.
2016-12-21 9:41 AM
Dear
Waclawek.Jan
,You can reviewthe
Description of STM32F0xx HAL and Low-layer driversBest Regards
Imen
2016-12-21 9:41 AM
Dear
Waclawek.Jan
,You can reviewthe
Description of STM32F0xx HAL and Low-layer driversBest Regards
Imen
2016-12-21 11:32 AM
Imen,
Thanks for the hint.
Threw on me a 1300-page (most of it doxygen-autovomited) pdf to keep me busy, huh? ;)
So on page 67 I found:
'x' corresponds to the group index and refers to the index of the modified register on a given bus.
Ah....a bit of reading of RM0091... I now understand. There is a single APB bus in the 'F0x, but there are quite a lot of peripherals on it so that the enable/reset RCC registers have been split (there are 31 active bits in them, incidentally, which would fit into a single 32-bit register; the reserved spaces between bits hint that there is an upward expansion plan). So the x in GRPx is the same x as in the RCC_APBxENR (and 'RSTR).
If you ask me, this is again a poor choice of register naming, as it is inconsistent. The same x in RCC_APBxENR in other STM32 families indicates the number of APB bus; when the bits for one bus are split this is indicated as y in RCC_APBxENRy - see e.g. RM0351.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.