2015-10-15 10:51 PM
Hello.
I'm trying to use DMA for graphic LCD control on F429(STM32Cube_FW_F4_V1.8.0).LCD spec is 160x128 and color is 16bit(RGB565) and bus type is 8bit parallel.So I'm using FMC to access LCD and now it's working well and I need to improve LCD update speed.Actually if I increase AHB/SYS clock, its bus clock is increasing so could manage to get fast LCD update but I should increase its clock speed so I'm trying to use DMA to improve its speed. (I think DMA will clear my problem, isn't it?)I wrote LCD_Write_DMA API to send color data to LCD and testing but it didn't send any data to LCD, external device.My API code is like as below...++++++++++++++++++++++++++++++++uint16_t dma_color;static void LCD_Write_DMA(uint16_t word, uint32_t word_len){ dma_color = word; /* DMA controller clock enable */ __DMA2_CLK_ENABLE(); /* Configure DMA request hdma_memtomem_dma2_stream0 on DMA2_Stream0 */ hDma2Stream0.Instance = DMA2_Stream0; hDma2Stream0.Init.Channel = DMA_CHANNEL_0; hDma2Stream0.Init.Direction = DMA_MEMORY_TO_PERIPH; hDma2Stream0.Init.PeriphInc = DMA_PINC_DISABLE
; hDma2Stream0.Init.MemInc = DMA_MINC_DISABLE; hDma2Stream0.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hDma2Stream0.Init.MemDataAlignment = DMA_PDATAALIGN_HALFWORD; hDma2Stream0.Init.Mode = DMA_NORMAL; hDma2Stream0.Init.Priority = DMA_PRIORITY_HIGH; hDma2Stream0.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hDma2Stream0.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hDma2Stream0.Init.MemBurst = DMA_MBURST_SINGLE; hDma2Stream0.Init.PeriphBurst = DMA_PBURST_SINGLE; HAL_DMA_DeInit(&hDma2Stream0); HAL_DMA_Init(&hDma2Stream0); /* DMA interrupt init */ HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn); HAL_DMA_Start_IT(&hDma2Stream0, (uint32_t)&dma_color, LCD_DATA, word_len*2);}++++++++++++++++++++++++++++++++I keep calling LCD_Clear() to see there is a data coming out from bus but even though I changed some parameters, I couldn't manage to work with DMA.As I said, it's working well with FMD without DMA so init and LCD relates config/HW connection is correct.I could confirm srcAddr/dstAddr/DataLen is valid at DMA API but whenever I call ''LCD_Write_DMA'', I cannot see data coming from F427, there is no CS/RS/BUS/RD/WR signal coming.Could anyone help what I missing and wrong?Many thanks.BR.Louie Yang. #fmc-lcdWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.