2018-02-15 2:25 AM
Hi everyone,
I'm tryng to use DMA with ADC on STM32L051x6 MCU.
When i see the Memory dump at the memory address of variable i takes the correct value from ADC DR but DMAIrq doesn't work never
Can somebody help me?
Thanks in advance
bool LED_CURRENT_ADC_Init(void)
{ LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1); //Enable DMA Clock DMA1_CSELR -> CSELR &= 0xFFFFFFF0; //Remap of DMA channels to ADC LL_ADC_REG_SetDMATransfer(ADC1, LL_ADC_REG_DMA_TRANSFER_UNLIMITED); //Enable DMA transfer on ADC DMA1_Channel1 -> CPAR = (uint32_t) (&(ADC1->DR)); //Configure the ADC data register address DMA1_Channel1->CMAR = (uint32_t)(ADC_val); //Configure the memory address DMA1_Channel1->CNDTR = 1; //Configure the number of DMA tranfer to be performs on channel 1 LL_DMA_SetChannelPriorityLevel (DMA1, LL_DMA_CHANNEL_1, LL_DMA_PRIORITY_VERYHIGH); LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MODE_CIRCULAR); //Set mode LL_DMA_MODE_NORMAL LL_DMA_MODE_CIRCULAR LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_1, LL_DMA_DIRECTION_PERIPH_TO_MEMORY); //Set direction LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MDATAALIGN_WORD); //Set dimension LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_MEMORY_INCREMENT); LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PERIPH_NOINCREMENT); LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_1, LL_DMA_PDATAALIGN_HALFWORD); LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_1); LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_1);LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_1);
NVIC_EnableIRQ(DMA1_Channel1_IRQn); NVIC_SetPriority(DMA1_Channel1_IRQn, 1);LL_ADC_SetClock(ADC1, LL_ADC_CLOCK_SYNC_PCLK_DIV1);
LL_ADC_SetSamplingTimeCommonChannels(ADC1, LL_ADC_SAMPLINGTIME_7CYCLES_5); LL_ADC_SetResolution(ADC1, LL_ADC_RESOLUTION_12B); LL_ADC_SetDataAlignment(ADC1, LL_ADC_DATA_ALIGN_RIGHT); LL_ADC_REG_SetSequencerChannels(ADC1, LL_ADC_CHANNEL_3); LL_ADC_REG_SetContinuousMode(ADC1, LL_ADC_REG_CONV_SINGLE); //LL_ADC_REG_CONV_SINGLE LL_ADC_REG_CONV_CONTINUOUS LL_ADC_ClearFlag_ADRDY(ADC1); LL_ADC_EnableIT_EOS(ADC1);LL_ADC_Enable(ADC1);
while(!LL_ADC_IsActiveFlag_ADRDY(ADC1))
{}
return true;}#dma-adcSolved! Go to Solution.
2018-02-15 5:00 AM
The DMA Irq will not occur if the DMA transfers aren't actually occurring. Check the DMA for error flags.
Check the handler name matches the one in the vector table, and the linker binds correctly.
Don't see the array defined. Check WORD != HALFWORD
Perhaps the are some L0 LL examples you can review.
2018-02-15 5:00 AM
The DMA Irq will not occur if the DMA transfers aren't actually occurring. Check the DMA for error flags.
Check the handler name matches the one in the vector table, and the linker binds correctly.
Don't see the array defined. Check WORD != HALFWORD
Perhaps the are some L0 LL examples you can review.
2018-02-22 2:06 AM
thanks for the help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.