2014-06-24 12:06 PM
Hello,
I am using the STM32F4 discovery board. I have a project in which I have a timer which generate an interrupts @ 100Khz. In the ISR it stores a new value to a variable. Now how can I use the DMA to send this value to the DAC which is updated at the same rate.ThanksRegardsSameer #stm322014-06-24 1:16 PM
hi ,
i do it like this :#define BITDEPTH 12 // 12 bits DAC
#define SAMPLERATE (SYSCLK / (1 <<
BITDEPTH
)) // Best audio quality 192MHz / (1 << 11) = 46875Hz
// Initialise Timer2
void Timer2_Init(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
// Clock enable
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
// Timer2 init
TIM_TimeBaseStructure.TIM_Period
=
SYSCLK
/ SAMPLERATE;
TIM_TimeBaseStructure.TIM_Prescaler
=
0
; // 192Mhz tick (adjust per your clock)
TIM_TimeBaseStructure.TIM_ClockDivision
=
TIM_CKD_DIV1
;
TIM_TimeBaseStructure.TIM_CounterMode
=
TIM_CounterMode_Up
;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
// Timer2 enable
TIM_ARRPreloadConfig(TIM2, ENABLE);
TIM_Cmd(TIM2, ENABLE);
}
// *********************************************************************************
// Timer2 interrup and DAC2 init
void Mod_Int_Init(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef DAC_GPIO_Init;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC, ENABLE);
//---------------------------------------------
// init from Timer2 Interrupt
TIM_ITConfig(TIM2,TIM_IT_Update,ENABLE);
NVIC_InitStructure.NVIC_IRQChannel
=
TIM2_IRQn
;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority
=
0
;
NVIC_InitStructure.NVIC_IRQChannelSubPriority
=
0
;
NVIC_InitStructure.NVIC_IRQChannelCmd
=
ENABLE
;
NVIC_Init(&NVIC_InitStructure);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
DAC_GPIO_Init.GPIO_Pin
=
GPIO_Pin_5
;
DAC_GPIO_Init.GPIO_Mode
=
GPIO_Mode_AN
;
DAC_GPIO_Init.GPIO_Speed
=
GPIO_Speed_25MHz
;
DAC_GPIO_Init.GPIO_OType
=
GPIO_OType_PP
;
DAC_GPIO_Init.GPIO_PuPd
=
GPIO_PuPd_NOPULL
;
GPIO_Init(GPIOA, &DAC_GPIO_Init);
DAC_Cmd(DAC_Channel_2,ENABLE);
}
// *********************************************************************************
// Timer2 interrupt
void TIM2_IRQHandler(void)
{
if(File_Loaded != 0)
if(SoundBuffer.writePos != SoundBuffer.readPos)
{
// Output the Audio as mono (only DAC2 pin is free)
Sound_Out = (uint16_t)(((SoundBuffer.left[SoundBuffer.readPos] + SoundBuffer.right[SoundBuffer.readPos])) >> 1);
DAC_SetChannel2Data(DAC_Align_12b_R,Sound_Out);
SoundBuffer.readPos++;
SoundBuffer.readPos &= SOUNDBUFFERSIZE - 1;
}
Int_Count++;
// Clear interrupt flag
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
}
I hope it can help you .
It's a part from my st429 mod player.
Tou can get the full source on this page :
Cheers.
2014-06-24 1:17 PM
double post .. delete thisd one ...
2014-06-24 2:02 PM
If you're computing it in a periodic interrupt, could you not just write it to the DAC then? Otherwise you've got to pay particular attention to keeping the IRQ and DMA synchronized.
2014-06-25 11:04 AM
thank you all... U all guys are great. Also I would like to thank Clive separately for ur great help and amazing spirit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.