STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 F103 - TIMER CLOCK

Posted on June 24, 2014 at 13:09Hi allI am looking at programming the digital filter in the input stage of a TIM2 capture/compare channel.The filter is configured using the 'IC1F' bits in 'TIMx_CCMR1'The different bit configurations make reference t...

jamie by Associate II
  • 1470 Views
  • 2 replies
  • 0 kudos

STM32f4 internal pull down, external pull up

Posted on June 25, 2014 at 11:55Hi,I'm using an STM32F4 and have configured IOs as pwm outputs with internal pull down. These pins have been connected to an input of another chip which has a 5V pull up on its inputs. After some time the processor br...

thommagn by Associate II
  • 1224 Views
  • 1 replies
  • 0 kudos

USB device and CDC class

Posted on June 17, 2014 at 11:31Hi all,I'am using USB device CDC class to communicate datas with a host. But I've a strange problem. (I'am using the STM32F429i Disco platform)The STM32 code create a memory area with 00 01 02 03 04 ... datas and then...

vincent2 by Associate II
  • 1234 Views
  • 1 replies
  • 0 kudos

Digital Value to DAC

Posted on June 24, 2014 at 21:06Hello,       I am using the STM32F4 discovery board. I have a project in which I have a timer which generate an interrupts @ 100Khz. In the ISR it stores a new value to a variable.        Now how can I use the DMA to ...

STM32CubeMX wrong pin label

Posted on June 25, 2014 at 15:47Hi,Using STM32F405RGTx, pin 64 is labelled PDR_ON while datasheet contains VDD.Which one is the correct one ?Thanks.

STM32F334: the new STM32 Digital-Power Microcontroller

Posted on June 25, 2014 at 17:29ST’s new microcontroller http://www.st.com/web/en/catalog/mmc/SC1169/SS1576/LN1820 simplifies transition to energy-efficient digital power supplies by providing all the major power-control functions in a single chip. ...

STM32F401 reference manual

Posted on June 25, 2014 at 15:07I'm sure that this is a really silly question, but is there actually a reference manual for the STM32F401 chips? I can't see one on the design resources page. The STM32F401 Discovery documentation refers to ''RM0344''...

evan2 by Associate II
  • 1615 Views
  • 2 replies
  • 0 kudos

Sequence of ADC conversion in Regular Simultaneous Mode

Posted on June 18, 2014 at 14:34Hi Everyone In my project, I need to capture 6 channel ADC signals in Regular Simultaneous Mode. for that, I just started for 2 channels (Channel 0 in ADC1 & Channel 1 in ADC2). Since it does simultaneous conversion, ...

ss2 by Associate II
  • 3564 Views
  • 8 replies
  • 0 kudos

PDR_ON connection question

Posted on May 28, 2014 at 07:31We are using the controller STM32F427ZIT6 from ST in our design. As we are using the NRST pin for processor reset in our older design(Atmel AT91FR40162S-CJ) we are trying to Bypass the Internal Reset circuitry of ST.In...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.