2018-04-26 1:16 AM
Hi,
The port.c file for the same FreeRTOS version [8.2.3] have a difference.
In the Official FreeRTOS release: configPRE_SLEEP_PROCESSING( xModifiableIdleTime ); configPOST_SLEEP_PROCESSING( xExpectedIdleTime ); In the STM32CubeMX configPRE_SLEEP_PROCESSING( &xModifiableIdleTime ); configPOST_SLEEP_PROCESSING( &xExpectedIdleTime ); Why this difference? It is wrong in the Cube? Best Regards, Sergio2018-04-26 8:15 AM
https://www.freertos.org/low-power-ARM-cortex-rtos.html#using_mcu_specific_features
are macros, not functions, so are inlined with the calling code. The parameter, xModifieableIdleTime, is therefore accessible directly inline, not as a function parameter. Therefore the addition of the '&' is not necessary, even if the address of the variable is needed, as the address of the variable can be directly accessed in the implementation of the macro instead of where the variable is passed as a parameter to the macro.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.