2025-08-14 10:30 AM
Hello... I'm learning to use an external ST-Link to debug the F446ZE Nucleo using SDW. Can anyone advise on how to connect the SDIO, SDW pin on the Nucleo board to the external ST-Link v2? Additionally, what settings should I configure in CubeIDE to use the ST-Link v2? I also have an ST-Link v3. Any advice on ST-Link v3 is also welcome, thank you.
2025-08-16 3:04 PM - edited 2025-08-16 3:08 PM
On the Nucleo-H743 the MIPI connector for external ST-LINK V3 is documented in the user manual for the board UM2407, table 5.
The connector is called "STDC14". A suitable cable usually comes with the ST-LINK V3 MINIE.
It is extension of "MIPI10" debugger cable/connector: it has two extra pins on each side, two of them are for the target UART (TTL RX & TX), other two are NC. You can use a MIPI10 cable but won't have the UART connection.
Enjoy.
2025-08-16 5:25 PM
yes i saw an extra 2-pin on the STLINK v3, if that's for UART Tx and Rx then i probably don't need it, cos i m using for flashing and debugging the program.
What are the configurations needed on the CubeIDE?
2025-08-19 4:29 AM
> What are the configurations needed on the CubeIDE?
In the Cube, Pinout view: Trace and debug-> Debug-> Serial Wire.
This will reserve the pins used by the debugger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.