2019-11-24 9:11 PM
Hi,
i'm trying to flash the STM32H743I_EVAL example into the Nucleo-H743Zi.
But couldn't able to flash into the Nucleo.
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 8000 kHz
Info : STLINK v3 JTAG v2 API v3 M1 VID 0x0483 PID 0x374E
Info : using stlink api v3
Info : Target voltage: 3.296192
Info : Stlink adapter speed set to 8000 kHz
Info : STM32H743XIHx.cpu0: hardware has 8 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x08002d40 msp: 0x20020000
Info : Stlink adapter speed set to 8000 kHz
adapter speed: 8000 kHz
Info : Device: STM32H7xx 2M
Info : flash size probed value 2048
Info : STM32H flash has dual banks. Bank (0) size is 1024kb, base address is 0x8000000
Info : Device: STM32H7xx 2M
Info : flash size probed value 2048
Info : STM32H flash has dual banks. Bank (1) size is 1024kb, base address is 0x8100000
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected
This is my log file. someone please help me get me through this.
Thanks,
Vimal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.