STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debug works, run causes Hardfault

Hello,I've got a realy strange issue. I'm using an STM32F107, with SW4STM32 and CubeMX. The controller is on a custom board. When I click on "Run" in eclipse, the controller is not starting. It seemed, that he's going immediately in a HardFault. Even...

user 143 by Associate III
  • 1164 Views
  • 1 replies
  • 0 kudos

Debugging not happening on Nucleo-H743Zi

Hi,i'm trying to flash the STM32H743I_EVAL example into the Nucleo-H743Zi.But couldn't able to flash into the Nucleo.Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)Licensed under GNU GPL v2For bug reports, read http://openocd.org/d...

VPras by Associate II
  • 875 Views
  • 0 replies
  • 0 kudos

STM32F103 Npulses example

Hello. In order to drive a stepper motor with CanBus, I want driver a L6208. I would use a timer to generate Npulses. I've read AN4776 (General-purpose timer cookbook ) but I don't understand somethink, I can't run the timer.Any people have example c...

jihzed by Associate II
  • 2182 Views
  • 3 replies
  • 0 kudos

I'm using 4 ADC channels and sending the data to a DMA buffer. The data from the different channels are interfering with each other and i'm not sure why. The goal is to read from PA0, PA1, PA4, and PA5 at the same time. so i may going about it wrong.

my data for this looks like the following without giving inputPA0 PA1 PA4 PA50 250 216 190I expect this PA0 PA1 PA4 PA50 0 0 0and when i start giving channel PA0 data wit...

Paulset by Associate II
  • 2905 Views
  • 6 replies
  • 0 kudos

Resolved! Push button problem on STM32F407G-DISC1 board

What is wrong with my code? The code never hits the turn on led part when I press the B1-USER1 button. From the board manual there is a LED on PD13 and the user push button on PA0.#include "stm32f4xx.h"     GPIO_InitTypeDef GPIO_InitDef;   int main(v...

Test User by Associate III
  • 1003 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.