2014-02-23 10:14 AM
Hello,
I use TIM1 to generate a clock-signal at the gpio-output-pin TIM1_CH1. This signal will be generated until a rising edge is detected at TIM_ETR (gpio-input). So the output-signal will be immediately pulled down to low as you can see in screenshot (after a detected TIM_ETR). So far, so good.
This really short pulse with an immediately low after the rising edge is to fast (you can see it in the attatched screenshot). So I try to expand/stretch the last pulse with a dead-time insertion. But this is not working at me.
I hope somebody can hint me.
{ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; TIM_BDTRInitTypeDef TIM_BDTRInitStructure; /* TIM DISABLE counter */ TIM_Cmd(TIM1, DISABLE); /* System Clocks Configuration */ /* TIM1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /* Time base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Period = 72; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Output Compare Toggle Mode configuration: Channel1 */ TIM_OCStructInit(&TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM1, &TIM_OCInitStructure); /* enable the choose to stop the timer on rising/falling edge at external * pin PA12 (=CAM_READ) */ TIM_ClearOC1Ref (TIM1, TIM_OCClear_Enable); TIM_ETRConfig (TIM1, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); /* down HERE !!! seems to be my problem ??? */ /* ==================> */ /* Automatic Output enable, Break, dead time and lock configuration*/ TIM_BDTRStructInit(&TIM_BDTRInitStructure); TIM_BDTRInitStructure.TIM_OSSRState = TIM_OSSRState_Disable;//TIM_OSSRState_Enable; TIM_BDTRInitStructure.TIM_OSSIState = TIM_OSSIState_Enable; TIM_BDTRInitStructure.TIM_LOCKLevel = TIM_LOCKLevel_OFF; TIM_BDTRInitStructure.TIM_DeadTime = 72; TIM_BDTRInitStructure.TIM_Break = TIM_Break_Disable; TIM_BDTRInitStructure.TIM_BreakPolarity = TIM_BreakPolarity_Low; TIM_BDTRInitStructure.TIM_AutomaticOutput = TIM_AutomaticOutput_Enable; TIM_BDTRConfig(TIM1, &TIM_BDTRInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Disable); TIM_CtrlPWMOutputs(TIM1, ENABLE); }2014-02-25 4:25 PM
Reading in datasheet and application_notes does not solve my problem. I hope someone can give me a little hint.
2014-02-26 1:12 AM
You can't do that. You did not mention which model are you using, so look for example at RM0090 rev.6 (for 'F4xx) fig.114 - the ETR input throttles the OC1Ref signal, while the positive/negative ''splitter'' where the dead time insertion happens comes after this.
[EDIT] I take this back - this is the reason why dead time insertion *can* be used to make a pulse longer. However, looking at Fig.120 in the same RM0090, to delay OCxRef's trailing edge, OCxN output has to be utilized (and perhaps inverted, by setting CCxNP=1). Note, that all pulses then be longer. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.