2012-11-09 8:55 AM
Server Error in '/' Application. The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases.
Description: An unhandled exception occurred during the execution of the current web request. Please review the stack trace for more information about the error and where it originated in the code.
Exception Details: System.Web.HttpException: The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases. Source Error: An unhandled exception was generated during the execution of the current web request. Information regarding the origin and location of the exception can be identified using the exception stack trace below.
Stack Trace:
[HttpException (0x80004005): The control collection cannot be modified during DataBind, Init, Load, PreRender or Unload phases.] System.Web.UI.ControlCollection.RemoveAt(Int32 index) +11110720 System.Web.UI.Control.AddedControl(Control control, Int32 index) +11036232 ST.App.MySTCom.Forums.WebParts.CommunitiesAllForums.RunAnonymous() +209 System.Web.UI.Control.EnsureChildControls() +146 System.Web.UI.Control.PreRenderRecursiveInternal() +61 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Control.PreRenderRecursiveInternal() +224 System.Web.UI.Page.ProcessRequestMain(Boolean includeStagesBeforeAsyncPoint, Boolean includeStagesAfterAsyncPoint) +3394
#forum-broken
2012-11-09 8:59 AM
Hopefully the database isn't fatally corrupted, but it appears to be melting down.
Suggest posters use the STM32 Discovery forum, as the STM32 forum is currently unreadable for posts made on 9-November-2012. I've attempted to contact a moderator.2012-11-09 9:43 AM
Also noted on the ''Forum related Functionality issues'' forum:
[DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/Functionality%20issues/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/STM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC568]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/Functionality%20issues/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fe2esupport%2fLists%2fFunctionality%20issues%2fSTM32%20Forum%20Server%20Error%20in%20%27%27%20Application&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000C1184011A4DEFF4BA0E41441DCAEC5682012-11-09 4:22 PM
im greeted with this page on most visits to this forum lol, drives me crazy!!!
2012-11-12 9:30 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.