2023-01-15 8:03 PM
안녕하십니까?
STM32H743�?� 예로 들 경우,
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
}
와 같�?� �?역�?� 있�?� 때, RAM_D1�?� 공간�?� 부족하여
.data 섹션�? 대해서 RAM_D1과 RAM_D2�? 할당하고 싶습니다.
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM_D1 AT> FLASH
�?� 부분�?� 어떻게 수정해야 하나요?
2023-01-17 1:44 AM
Hello @JongOk Baek
There are better chances to solve your issue when writing in English!
To help you, I translated your post :
How to allocate the .data area to two memory areas
Hello?
Taking STM32H743 as an example,
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
}
When there is an area as in, RAM_D1 is out of space
For the .data section, I want to allocate to RAM_D1 and RAM_D2.
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM_D1 AT> FLASH
How should I fix this part?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.