2017-12-13 7:19 AM
I’m really new in the use of the end-devices and I have some troubles to achieve a low consumption in sleep mode (I get 0,13mA).
I’m using in my end device the CMWX1ZZABZ-078 micro-controller with a Chipset: Semtech (SX1276) + STM (STM32L) which is the same micro-controller of B-L072Z-LRWAN1 LoRa Discovery kit (I also bought this card to start working with Lora). I use the example “LRWAN-NS1� from the I_CUBE_LRWAN which is an example to start a simple use of a LORA end-device.
I saw that it’s able to get something around 4uA which is something really useful for my project. I use a 2600mAh cell (I don’t have the equipment to measure the sending time). I have 3 currents in my Lora end-device ( 1.- Sleep mode: 0.13mA. 2.- Wake-up: 6,05mA. 3.- Data sending: 23mA.).
You can see my circuit in the attached file, so you can see that I connect the VDD_TCXO with PA12.
It’s been a couple of weeks that I’m trying to understand the sleep mode to be sure that I’m able to go lower than 0,13mA for a longer time life of my batteries. I appreciate any help you can give me to keep going with this end device.
Best Regards,
Jorge.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.