2015-11-28 9:00 AM
Hello all,
I made a new project with latests CubeMx 1.9 for stm32f4 My problem is that the autogenerated code does not trigger the ISR. I found out that when I__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
just before HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 1000, RTC_WAKEUPCLOCK_RTCCLK_DIV16); in the MX_RTC_Init() function, then it works as ecpected. Seems that WUTF flag unintentional set and that will block any further timouts to not activate the ISR. Bug or feature? I would call it bug. Regards, Adib. #!stm32-!cubemx-!rtc-!timeout2015-12-03 3:15 AM
Hi adib,
Which line of STM32F4 are you using? and Which low power mode are you experimenting? Also you should upgrade to the latest Version 4.11.0 of STM32CubeMx. Referring tohttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/DM00068628.pdf
of STM32F427/437 and STM32F429/439, there is a limitation related to the wake up sequence from Stand by mode (section 2.1.3) that lead the user to clear all related wake up flags before enabling sources.This limitation is not taken into account in the generated code by STM32CubeMx.This issue is reported to dedicated team. Sorry for inconvenience it may bring-Shahrzad-2016-04-12 5:34 AM
Dear user,
This issue is now fixed by adding in MX_RTC_Init(): __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF); Before the call to: HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 1000, RTC_WAKEUPCLOCK_RTCCLK_DIV16);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.