2016-06-03 2:29 PM
When import
an STM32CubeMX generated project under System Workbench for STM32 follow the instruction of
http://www.openstmorg/Importing+a+STCubeMX+generated+project
. Numerous errors shown:unknown type name 'GPIO_TypeDef'
'GPIOC' undeclared (first use in this function)
and so on.
In order to solve this problem, a macro definition
#define STM32F769XX
should be added
manually
Meanwhile, the STM32F769NIHx_FLASH.ld can't be complied because their is a error in line 55
_estack = %stack%; /* end of RAM */
it should be replaced to
_estack = 0x20080000; /* end of RAM */ then the project cancomplieswell.
2016-06-06 4:36 AM
Hello,
Can you please indicate which STM32CubeMX version are you using?Thanks.2016-06-06 5:08 AM
Hi,
The .ld file that the CubeMx generates for me (STM32F769NIHx_FLASH.ld) contains:_estack = 0x20080000; /* end of RAM */
I suggest you to use the last version of CubeMx v4.15 and update the toolchain.
Please let me know if this workaround resolves your issue or you still have error.RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.