cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.20.1 Properties does not appear

stephengoodman9179
Associate II
Posted on April 26, 2017 at 21:53

In CubeMX 4.20.1 I have opened a project from a previous version. Then when I go to edit the Properties... no window comes up!  If I open another project or create a new one, the Properties... window appears as expected.

How do I fix this? I need to review and possibly change the properties!

thanks!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee
Posted on April 27, 2017 at 11:19

Hi, 

Please share your .ioc to check this case.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on May 03, 2017 at 10:20

Hello

Liebman.Mark.002

,

I had a look to your point. I took an ioc from CubeMX4.0 and open it with CubeMX4.1.

I can open Project/Settings/, open the configuration of IPs etc...

What do you mean by properties? Is it Project Settings?

As I can't reproduce the issue and as Imen said, we need you to share your ioc to progress on this point.

BR. Eric

stephengoodman9179
Associate II
Posted on May 03, 2017 at 14:14

Yes, it was the project settings dialog which would not appear when selected from the menu. In that project it was never seen. If I see it again I will share.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.