cancel
Showing results for 
Search instead for 
Did you mean: 

cubeMX 4.14 does not work with IAR

tarzan2
Senior
Posted on April 12, 2016 at 17:18

Hello

Compiling a test project for IAR:

Could not open file: 'E:\temp\cube4.14\test\EWARM\E:\Prog\STM32CubeMX_repo\STM32Cube_FW_F4_V1.11.0\Drivers\CMSIS\Device\ST\STM32F4xx\Source\Templates\iar\startup_stm32f439xx.s' 

useless strcat...

Resulting in a 1/2 lost day... I hope that this new version of cubeMX will solve my problem, this morning I was searching why the I2C module sometime brings SDA low. The afternoon I can't compile anymore...
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
slimen
Senior
Posted on April 13, 2016 at 10:03

Hi bonelli,

I think your path is not properly set up: 'E:\temp\....\E:\Prog' !

I have checked from my side and successfully open the file startup_stm32f439xx.s

To have more idea about I2C module and SDA, you can refer to the

http://www2.st.com/content/ccc/resource/technical/document/reference_manual/3d/6d/5a/66/b4/99/40/d4/DM00031020.pdf/files/DM00031020.pdf/jcr:content/translations/en.DM00031020.pdf

-ForumSTM32-

tarzan2
Senior
slimen
Senior
Posted on April 13, 2016 at 12:44

Hi bonelli,

Please share your .ioc file to have more details about your problem.

Regards

-ForumSTM32-

tarzan2
Senior
slimen
Senior
Posted on April 13, 2016 at 23:16

Hi,

I have also the wrong path when I copy the .ioc in other repository and re-generate it (concatenate previous/original .ioc location with new one) !

Maybe you can try to generate your project in new and clean repository (without copy .ioc or generating in old path)

Regards

tarzan2
Senior
Posted on April 14, 2016 at 10:53

This is what I do with the previous test folder.

I retried 2 times (STM32F4 & STM32L4), always in a clean folder, the problem is the same.

tarzan2
Senior
Posted on April 14, 2016 at 14:20

Please note that I tryed with an other computer, fresh installation of cubeMX => same results, paths are corrupted.

COULD ST PROVIDES OLDER VERSIONS OF CUBEMX ?

Because this one is NOT working with professional tools such IAR. So ALL my projects are waiting and as a professional this is NOT acceptable.

stm32cube-t
ST Employee
Posted on April 15, 2016 at 10:07

Dear user,

This problem is under investigation. As a workaround, perform a ''Save Project as'' then generation is ok.

Best regards

stm32cube-t
ST Employee
Posted on October 06, 2016 at 17:31

Dear user,

This issue has been solve in STM32CubeMX 4.16.

Best regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.