STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube FatFS FreeRTOS double generated init code

Posted on March 17, 2016 at 15:55STM32Cube_FW_F4_V1.11.0  I have enabled 3 FATFS: SDRAM, SRAM and SDCard Bug 1: Using FreeRTOS and FATFS and USB-Desice on stm32F429 double generates   MX_FATFS_Init();  MX_USB_DEVICE_Init(); in ''main()'' and in Tas...

bernd2 by Associate
  • 11101 Views
  • 1 replies
  • 0 kudos

[Bug] CubeMX 4.14 and clock configuration issue

Posted on March 22, 2016 at 16:16The latest CubeMX 4.14 seems to have a severe issue with the clock configuration. In some situations it can't find the right clock configuration for a wanted frequency, and it starts an infinite search with no succes...

carmine by Associate II
  • 1539 Views
  • 2 replies
  • 0 kudos

cubeMX 4.14 does not work with IAR

Posted on April 12, 2016 at 17:18HelloCompiling a test project for IAR:Could not open file: 'E:\temp\cube4.14\test\EWARM\E:\Prog\STM32CubeMX_repo\STM32Cube_FW_F4_V1.11.0\Drivers\CMSIS\Device\ST\STM32F4xx\Source\Templates\iar\startup_stm32f439xx.s' u...

tarzan2 by Senior
  • 2602 Views
  • 9 replies
  • 0 kudos

[CRC] CRC Default poly cannot be disabled

Posted on April 15, 2016 at 15:10I cannot disable the default CRC polynomial when configuring the CRC peripheral from the Cubem MX (rev.4.13 with SRM32F030) combo box.is this a bug of Cube or I cannot realyy do this?thanks

stanzanim by Associate III
  • 855 Views
  • 3 replies
  • 0 kudos

Bug erport Cube & pinname starting with number

Posted on April 28, 2016 at 17:35Hi,There is a bug when I have the name of pin starting with number (e.g. 485_Power) then Cube creates defines like:#define 485_Power_Pin GPIO_PIN_6#define 485_Power_GPIO_Port GPIODwhich is not confirm with C/C++ stan...

Osto by Senior
  • 748 Views
  • 2 replies
  • 0 kudos

CubeMx 4.15.1 bug report ADC DMA Alignment

Posted on June 21, 2016 at 01:48Hi DMA with adc when configured has half word is generated and save has byte. Reproduction : - new project stm32l152ZDTx - ACtivate adc IN0 - add DMA transfert and set it to half word (default value by the way). - ope...

JulienD by Senior
  • 788 Views
  • 2 replies
  • 0 kudos

Can reset option bytes, STILL can't load firmware

Posted on October 02, 2016 at 20:39I have a very basic F103VET dev board, with the schematic. The board arrived running what I guess was ST-Link, which I don't use.  I was able to erase the Flash using the latest FlashLoader (FL) v2.8, via the Cmd l...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.