2015-09-16 2:01 AM
Hello, please give me the procedure to creat a project virtual com port(usb cdc) with STM32CubeMX. (STM32F429discovery)
I followed the steps but according to manager level péréphirique the material is unknown:Procedure(Using Win 7, STM32CubeMX Version 4.5 STM32Cube V1.0, Keil IDE 5.13.0.0 and STM32F429IDiscovery board):1. Open STM32CubeMX, Select Board Selector tab, Type of Board = Discovery, Reference = 32F429IDiscovery. 2. Pinout->Clear Pinouts.3. USB_OTG_HS, Internal PHY = Device Only4. Perhipherals - RCC, High Speed Clock (HSE) = Crystal/Ceramic Resonator5. MiddleWares - USB_Device, Class for HS IP = Communication Device Class (Virtual Comm Port).5. Project Settings -> Set Project Name = ''CubeProject''(arbitrary), Project Location, Toolchain (in my case MDK-ARM4.73).6. File->Save Project. 7. Project->Generate Code.8. Open Project. Opens Keil IDE 5.13.0.0 in my case. 9. Keil IDE asks me if I want to migrate the project from MDK version 4 to MDK version 5, which I elected to do. 10.Left click to select the ''CubeProject Configuration'' tab in the leftmost tree, Right click to bring up context menu, select Options forTarget ''CubeProject Configuration''. 11. On ''Target'' tab change Xtal Mhz from 12.0 to 8.0. 12.On ''Debug'' tab click settings(in top right corner), change Port fromJTAG to SW. Click the ''Flash Download'' tab. Add STM32F4xx 2MB Flash.Press OK. 13. Press OK again to exit options.14. OpenApplication/MDK-ARM folder, edit startup_stm32F429xx.s, change Heap_SizeEQU from 0x00000200 to 0x00000400. Save the file. 15. Project->Build target, to compile project.16. Connect pc to usb mini on discovery board(for code download). Connect pc to usb micro on discovery(for VCP). 17. Flash->Download, to download to board. 18. Reset the board. Click black push button knob or unplug and reconnect usb mini cable from board. 19.Check Device Manager in Windows, you should see under Ports(Com &LPT) an entry for STMicro Electronics Virtual Com Port (COM##).2015-09-16 5:51 AM
Hi med_yassine.jebabli,
1-Upgrade STM32CubeMx to versionhttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber
2-Upgrade STM32CubeF4 to version According to steps that you followed 3-Open STM32CubeMX, Select Board Selector tab, Type of Board = Discovery, Reference = 32F429IDiscovery. 4-You do not need to clear pinouts 5- USB_OTG_HS, Internal PHY = Device Only 6- Perhipherals - RCC, High Speed Clock (HSE) = Crystal/Ceramic Resonator 7- MiddleWares - USB_Device, Class for HS IP = Communication Device Class (Virtual Comm Port). 8-Configuration view: in connectivity USB_HS: set parameters as you like 9-Project Settings -> Set Project Name = ''(arbitrary)'', Project Location, Toolchain .. 10-Change the heap valueto 0x4000 as mentioned in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/problem%20in%20virtual%20com%20port&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx¤tviews=43]post -Shahrzad-2015-09-17 4:07 AM
2015-09-17 4:33 AM
2015-09-17 10:27 AM
Hi med_yassine.jebabli,
1-You wrote that you dowloaded CubeMx 4.5.0? but the latest version is 4.10! 2-Did you test an example with virtual com port from the latest package? If this example works and your project does not, maybe you have a hardware problem. 3-Did you install the virtual port com driver on your PC? -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.