STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

jump to specific location

Posted on September 14, 2015 at 17:31Hi. I have a problem with jumping to specific location on stm32 flash memory. At that location some functions should be implemented and the result from these functions have to be kept in any of (all purpose)regis...

Blink program not working

Posted on September 18, 2015 at 09:38Hi to all, I tried my first program on STM32F0 discovery board and I encountered some problems. My intention is to make LED3 and LED4 blinking, so I create a main program with system initialization and a LED clas...

STM32l052 Vrefint 2048 problem

Posted on September 18, 2015 at 08:52Hi. I try to measure internal voltage and temperature. The first measurement of the both is good. In all the others voltage is 2048, while temperature is ok. The controller uses MSI 2000000MHz. The measurement o...

baev_al by Associate III
  • 597 Views
  • 0 replies
  • 0 kudos

Infinite_Loop problem with STM32F030CCT6

Posted on September 18, 2015 at 00:31Hi all ST users.We have just replaced the STM32F030C8T6 microprocessor on some of our working boards to upgrade them with the larger STM32F030CCT6. A difference that should be both pin-compatible, periphiral comp...

0690X000006034ZQAQ.jpg

STM32F746IGT: Booting from FLASH Sector 4

Posted on September 10, 2015 at 23:46Hello all,I am looking how I can flash my firmware to sector 4 (0x0802 0000) and jump to it to execute the code.  I am using Keil uVision 5 as development environment.I know that I must changed the address in the...

keaven by Associate II
  • 815 Views
  • 2 replies
  • 0 kudos

Power management circuit for STM32F103

Posted on June 01, 2012 at 10:59Dear all,I need to design a board based on STM32F103RE.My board need to be powered in two ways, USB & Li-Ion 3.7V battery. In addition i need to design a IN-BUILT battery charging circuit( USB to Li-Ion battery) for t...

harinath by Associate III
  • 2937 Views
  • 2 replies
  • 0 kudos

creat project virtual com port

Posted on September 16, 2015 at 11:01Hello, please give me the procedure to creat a project virtual com port(usb cdc) with STM32CubeMX. (STM32F429discovery)I followed the steps but according to manager level péréphirique the material is unknown:Proc...

med by Associate II
  • 2290 Views
  • 4 replies
  • 0 kudos

HAL gpio libary code bug

Posted on September 04, 2015 at 09:24This problem has been reported in the following link.https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%...

dan2 by Associate II
  • 3300 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.