2008-06-23 2:25 AM
Converting temperature
2011-05-17 3:37 AM
I'm using the temperature sensor in my SMT32f103. It is configured in the following way:
Quote:
// ADC1 configuration ADC_DeInit(ADC1); ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); // ADC1 regular channels configuration // Micro internal temperature sensor ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_239Cycles5); It looks seems properly (aparently) and I get values from the ADC about 1715. When I convert this value to celsius I obtain 36C that is too much even for the processor temperature. I use the formula and the values from the datasheet. Those values are: Avg_slope = 4.3 mV/C V_25 = 1.4 V V_ref = Vdda = 3.3V Are those values right? How could I get real values? Thanks.2011-05-17 3:37 AM
temp C = (1.4 - 1715/2^12*3.3)/.0043 + 25
= 0.01828/.0043 + 25 = 4.25 + 25 = 29.25 C +/- 1.5 deg C sounds about right2011-05-17 3:37 AM
Your right it is a very wide range
V25 Avg_Slope Deg C 1.34 0.004 14.5715332 1.43 0.0043 36.22933321 1.52 0.0046 55.06220279 looks like the part to part variation is very high, but once calibrated, it's +/- 2deg. I guess you need to calibrate each part, power up and quickly take a reading at room temp (before it heats up), it should be 21 deg (or whatever your room temperature is). Compute a bias, store it in FLASH, and add that to any future reading and you should be ok.2011-05-17 3:37 AM
My value for V25 is 1.43. In the manual the value is between 1.34 and 1.52 but very small variations of this value imply big variations in the result. How could I get a better calibration of this value?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.