2019-03-17 3:48 AM
Hi
I want to connect printer to stm32f4 discovery board but i dont know form where i should start!
I connect keyboard to board successfully with stmcube hid library
for printer which usb host class should i select!?
regards
2019-03-17 3:58 AM
Printer Class
https://www.usb.org/defined-class-codes#anchor_BaseClass07h
I don't use Cube/CubeMX but as far as I know it's not something you can simply "select" there so you might need to write it yourself, or get a 3rd party library.
https://community.st.com/s/question/0D50X00009XkaNSSAZ/usb-printer-class
JW
2019-03-17 1:37 PM
Maybe old parallel printers are suitable to your application.
There are old endless-paper needle printers, ink printers, laser printers and cash-register-printers with this interface available.
Some special printers like those cash register printers and similar are produced up today with a parallel port interface.
For simple text printing the protocol is *very* easy. 8 datapins and 1 strobe pin. You apply the ASCII code for the character on the 8 datapins and issue a rising or falling edge (don't remember exactly) at strobe and this character will be immediately printed.
2019-04-08 12:20 PM
thanks for your reply
Do you have any tutorial!?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.