2017-09-28 9:42 AM
I'm a noob and I actually have two problems.
First, I'm trying to connect a SPWF04SA board to a WPA2 protected network using micropython. From some examples I have found on the micropython website it looks like I should be able to use the statement:
wlan.connect('PE9000',(WLAN.WPA2,'xxxx'))
But I get the error:
Traceback (most recent call last):
File '<stdin>', line 1, in <module>
AttributeError: type object 'WLAN' has no attribute 'WPA2'
How do I specify WPA2 security when trying to connect?
My second problem is probably my own doing. After playing with the board for a while it started acting a little flaky so I tried resetting it with the command AT&F. Now, however, I can no longer start the python shell. I get the error:
ERROR:16:Cannot switch to Python shell
I have tried re-enabling the console with AT+S.SCFG=console_enabled,2 but it still doesn't work. How do I get this working again? Note the board came 'python enabled' and I haven't changed any of the jumper settings.
Thanks for any help.
#wpa2 #micropythonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.