2015-03-04 5:06 AM
Dear Sir:
I can't connect a STM32F427IIT6 custom board via ST-link (SWD) of STM32F407 discovery board . Neither through uVision 5.0 nor through ST-link Utility (I use STM32 ST-link utility v3.6.0, STLinkUSDDriver.dll v4.3.4.0, ST-link-CLI.exe v2.2.0). When try connecting using ST-link utility, it will report:No target connected
Can not connect to target!
Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu. The question is: Q1: Can STM32F407 discovery ST-link be used for STM32F427 body? Or Only STM32F427 discovery board can be connected with! Q2: If yes for STM32F407 discovery board, what ST-link FW version is fine to used on STm32F427 device? Q3: What hardware should I check when connected by SWD? Now on discovery board, I remove two jumps of CN3, and connect only pin 2~4 (SWD_CLK, GND, SWD_DIO) of CN2 to (PA14, GND, PA13) of STM32F427 custom board.
2015-03-04 7:28 AM
1) Should be fine
2) Use current firmware, also should be fine 3) You must disconnect local target, ie remove CN1 jumpers, and any related Solder Bridges. I would connect NRST to the new target.2015-03-08 6:28 PM
Dear Clive1:
Thanks for the information. Now I can connect/download FW/run via ST-Utility.exe to target board. However uVision still can't recognize the target board. Maybe it's due to device ID mismatch between project setting in uVision and real chip. Q: Is there easy way to change device setting in project? Or I need to ceate a new project always when I want to change device setting? It shows grey color in project setting.2015-03-09 4:45 AM
I'm not sure what you're asking, the options for the project should be changeable, do you have a screen shot illustrating the problem?
Check if the ST-LINK is configured in SWD mode under the debugger settings.Make sure the project template, or whatever you're using as a starting point is not read-only.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.