2024-11-28 12:06 PM
Hello,
I’d like to configure two UCPD ports on STM32G0B1 in STM32CubeMX. I’m working on a custom board with two TCPP03-M20 (dual role). However, I’ve noticed that STM32CubeMX seems to support configuring only a single UCPD interface. I’ve tried setting it up, but I can’t figure out how to make it work for both ports. Is it possible to configure both UCPD interfaces manually in the code, or am I missing something in CubeMX? Any guidance or examples would be greatly appreciated.
Thanks
Vladislav
2024-12-02 10:43 PM
Hello Vladislav.Sedlak
Please Migrate to STM32CubeMX-6.13.0, where issue has been resolved.
You will find attached the .ioc of an example with configuration of both UCPD of the STM32G0B1 in dual-role mode.
Best regards
Pascal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.