2014-03-26 5:01 AM
Hi all, your thoughts on this would be appreciated.
I have a need to re-configure the SWCLK pin on the STM32F103C8 (PA14) as an input with pull-up. By default on power up it is input puul-down. I still intend to use as SWCLK for my SW Debug. I tried reprogramming the GPIOA_CRH and GPIOA_ODR registers to set this, but it had no affect on what the pin physically did. As an experiment, I changed the MAPR to completely disable JTAG, thus release PA14. Now, changing GPIOA_CRH and GPIO_ODR correctly affects what the pin does. OK, so I can accept that whilst the JTAG is enabled, that modifying the PulUp/PullDown status may not take affect, but what is strange is that if I: Disable JTAG Set PA14 as Pull Up Re-enable JTAG then the SWCLK pin retains the state I re-programmed it to. Indeed after this sequence I can change the mode of the pin as I wish. So taking this one step further i tried Disable JTAG Re-enable JTAG(SWD only) Modify PA14 input mode and this works as expected. So it appears you have to disable jtag, then re-enable before you can modify the input mode of the pin. This seems very odd does it not? EDIT Have now realised that disabling the JTAG pins then re-enabling the SWD pins doesn't work - it appears theat when I do this, the SWD interface is non functional (unless the SWD tries to communicate wilst NRST is active, which I cannot do). Almost as if once you turn the pins off, they remain off until reset! Nick #stm32f103-swd-swclk-afio-maprWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.