2017-07-09 10:45 AM
Does anyone know how to configure the Nucleo-L496ZG-P for SMPS operation, specifically to run the supplied example PWR/PWR_RUN_SMPS/Src/main.c
#smps #l4962017-07-09 11:01 AM
PWR/PWR_RUN_SMPS/readme.txt
2017-07-10 11:09 AM
I am afraid the readme.txt file does not explain how to modify the target board to run this example. The board guide says by default SMPS is disabled and it is. I could spend a day a figure out how to modify it but thought the instructions should be in the readme.txt file since the modification appears to be complicated and was intended to be used in a specific way.
2017-07-10 6:34 PM
Where do you get the idea that modifications to the board need to be done? Try building and running the supplied examples.
2017-07-10 6:54 PM
You are right, took out the jumper I put on and it still worked. Checked a 2nd board and it worked. I must have had something wrong with my build the first time. Thanks for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.