2017-06-28 8:51 AM
I use BSP/STM32469l-Discovery (from STM32CubeMx) , and use STM32F4xx_HAL_Driver to do a small project like this video :
https://www.youtube.com/watch?v=u_TVAudWabI
(I convert evaluation board from STM32F429-Disco to STM32469-Disco)But I got some error like:
LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_ConfigPhyTimer (referred from stm32469i_discovery_lcd.o).
LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_ConfigVideoMode (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_DeInit (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_IRQHandler (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_Init (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_LongWrite (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_ShortWrite (referred from stm32469i_discovery_lcd.o).LCD_TEST\LCD_TEST.axf: Error: L6218E: Undefined symbol HAL_DSI_Start (referred from stm32469i_discovery_lcd.o).Not enough information to list image symbols.Finished: 1 information, 0 warning and 8 error messages.'LCD_TEST\LCD_TEST.axf' - 8 Error(s), 0 Warning(s).It seems that
stm32469i_discovery_lcd.c cannot link to HAL(stm32f4xx_hal_dsi.c).
But In complie section , I found all require obj file create.
My stm32f4xx_hal_dsi.c version is V1.7.1
My stm32469i_discovery_lcd.c version is V2.0.0
My MDK-ARM version is V5.23
Solved! Go to Solution.
2017-06-28 8:26 PM
I found the reason why BSP fail to link.
Because it need to define symbol in preprocessor ( HAL_DSI_MODULE_ENABLED).
2017-06-28 9:15 AM
Hi
chou.dai
,Please refer to this document, this may help you to integrate BSP library:
https://community.st.com/0D50X00009bMM6QSAW
Regards
Imen
2017-06-28 8:26 PM
I found the reason why BSP fail to link.
Because it need to define symbol in preprocessor ( HAL_DSI_MODULE_ENABLED).
2017-07-10 9:14 AM
Hi , Dai chou !
I have a problem with the STM32F469I-Discovery with the BSP LCD as your problem. And I add HAL_DSI_MODULE_ENABLED & HAL_DMA2D_MODULE_ENABLED to the preprocessor. It resolves the problem as you described. However,it comes with the new problem 'Undefined symbol HAL_LTDCEx_StructInitFromVideoConfig (referred from stm32469i_discovery_lcd.o).'. Do you have any idea? Thx!
2017-07-10 6:47 PM
you could also just uncomment the module in stm32f4xx_hal_conf.h instead of the preprocessor directives, but either way, you still need to add the .h and .c files
STM32Cube_FW_F4_V1.16.0/Drivers/STM32F4xx_HAL_Driver/Inc/stm32f4xx_hal_ltdc.h and Src/stm32f4xx_hal_ltdc.c
there's also stm32f4xx_hal_ltdc_ex.h and .c to add.
you'll want to do this with DSI, DMA2D, LTDC, FMC [so you can use the SDRAM as frame buffer]
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.