2019-02-08 5:55 AM
Hi there,
i wondered if it's possible to support more than two composite device classes. I am using stm32f407ig and in the reference it says there is a control endpoint 0 and it supports 3 IN/OUT Endpoints. So it must be possible to implement CDC+HID+MSC or am i wrong?
Anyone has experience with composite and how to implement it the best way?
2019-02-09 5:01 PM
Sure, composite devices can have > 2 functions. The limiting factor is number of available endpoints.
-- pa
2019-02-10 11:26 PM
Any idea how to implement that because if I am right i think i need an extra driver for every combination of device? Like if i want 3 Device Endpoint then i need an extra driver
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.