2012-09-13 1:30 PM
I started learn about STM32f4 discovery and i want to send and receive some data between my discovery board and my PC before i was working with AVR and i was sending and receiving data with RS232 but now i want to find very simple way to sending and receiving data for example with USB .Can anybody help me.
Thank You2012-09-13 4:15 PM
USB != Very simple
Perhaps you should review the USB library code, like the CDC/VCP Here's a port to STM32F4-Discovery from the example's STM3240G-EVAL target.https://docs.google.com/open?id=0B7OY5pub_GfIdnREeExyRWNXbFE
2012-09-13 5:05 PM
Thank you for your help
I have another QuestionI have code for writing on USART and i want to use of printf sprinf etc. for writing my MSG on USART but it doesn't work.
Am i add some include to my code? this is my code:
#include ''stm32f4xx.h''
#include <stm32f4xx_usart.h>
#include <stdio.h>
/* Private macro */
/* Private variables */
/* Private function prototypes */
/* Private functions */
/**
**===========================================================================
**
** Abstract: main program
**
**===========================================================================
*/
#include <stm32f4xx.h>
#include <stm32f4xx_usart.h>
char g;
void init_usart(void){
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* enable peripheral clock for USART2 */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* GPIOA Configuration: USART2 TX on PA2 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART2 pins to AF2 */
// TX = PA2
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2, ENABLE); // enable USART2
}
void Delay(__IO uint32_t nCount)
{
while(nCount--)
{
}
}
int main(void){
init_usart();
//uart_puts(''Init complete!'');
while(1){
//printf(''iman:%i'',g);
USART_SendData(USART2, 'h'); // defined in stm32f4xx_usart.h
Delay(0x3FFF);
}
}
2012-09-14 1:03 PM
In Keil it can be done thusly
//******************************************************************************
// Hosting of stdio functionality through USART2
//******************************************************************************
#include <
rt_misc.h
>
#pragma import(__use_no_semihosting_swi)
struct __FILE { int handle; /* Add whatever you need here */ };
FILE __stdout;
FILE __stdin;
int fputc(int ch, FILE *f)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2, ch);
return(ch);
}
int fgetc(FILE *f)
{
char ch;
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET);
ch = USART_ReceiveData(USART2);
return((int)ch);
}
int ferror(FILE *f)
{
/* Your implementation of ferror */
return EOF;
}
void _ttywrch(int ch)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
USART_SendData(USART2, ch);
}
void _sys_exit(int return_code)
{
label: goto label; /* endless loop */
}
/**************************************************************************************/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.