2016-11-16 12:06 AM
Hello everyone,
I'm using a STm32F407 that communicates with an eeprom throught I2C. Although most of the time it's working fine when i'm running the code with the debugger(i have the ST link/V2 ISO) often the code gets stuck in this functionwhile (HAL_I2C_Mem_Write(&hi2c1, uchEEPromAddress, Mem, I2C_MEMADD_SIZE_8BIT, (uint8_t*)(buff + t), TX_I2CBUFFERSIZE, 1000)!= HAL_OK)
{
GetError(); // gets stuck sometimes
} This function does not return HAL_OK and it does not Timeout either
I saw that the code gets stuck in the function
/* Wait until BUSY flag is reset */
if(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY_FLAG) != HAL_OK)
{
return HAL_BUSY;
} Which is nested in the main
HAL_I2C_Mem_Write function.
Any ideas ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.