2013-03-26 4:43 AM
Hi Folks
I just thought that I would say that using the Code Red tools with the Discovery Board is quite simple:Move
the
soldered links on SB3 and SB7to
SB2 an SB6.The
n allthe
debugger signals are available onthe
headers CN2 and CN3 CN3 1,2,3,4 = VCC, SWCLK, GND, SWO and CN2 5,6 = RESET and SWO. This is a quite a good low cost development system #code_red #stm32-discovery #stm32f42013-03-27 5:34 AM
I need the support :)
I'm more HW than SW and have moved from Ardunio -> mbed -> ST32F4. its a bit of a crazy learning curve at the moment!!2013-03-27 9:29 AM
A personal (private) licence for Crossworks is about 1/10 of the above mentioned cost, so $150 approximately. I have one, and still view it as a good investment.
And the last time I checked CodeRed, they had limited licences for 256/512k codesize, at a price of $256 and $512 - what a coincidence ;) But as discussed, you need to check for the debug adapter support. CW supports both ST-Llink V1 and V2, but the former one not under Linux.2013-03-28 1:13 AM
...Yup looks like cross works is a better option if you are not doing commercial dev, however for commercial dev they are more expensive. (also I like to support open source if I can)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.