STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HardFault_Handler exception problem

Posted on March 27, 2013 at 23:32Hello all,I will apreciate any help that can give me some light to understand what is happening.The firmware has a loader, data flash and an application.ROM memory mapping:* Loader 0x0000h - 0x3FFFh* EEPROM DATA 0x...

juanjo by Associate II
  • 1344 Views
  • 2 replies
  • 0 kudos

Needed memory for embedded linux

Posted on March 28, 2013 at 07:12Hi,      I have to know whether how much amount of program memory will need to debug a Embedded linux in controller as well as needed RAM size to load the linux application. Am new to this platform, So could you plea...

Number of ADC channels in STM32F207Zx?

Posted on March 27, 2013 at 21:57Hi, Trying to get my head around how many ADC channels that are available in STM32F207Zx chip. Datasheet p14 Table3 claim ''Number of channels = 24''. Also on p.1 ''ADC with up to 24 channels''. OTOH, Reference manua...

optifier by Associate II
  • 3349 Views
  • 7 replies
  • 0 kudos

Code Red / Red Probe with the 32F4 DISCOVERY board

Posted on March 26, 2013 at 12:43Hi Folks I just thought that I would say that using the Code Red tools with the Discovery Board is quite simple:Move the soldered links on SB3 and SB7 to SB2 an SB6.Then all the debugger signals are available on the ...

bl by Associate II
  • 3949 Views
  • 12 replies
  • 0 kudos

How fast can the timer inputs count?

Posted on March 28, 2013 at 00:02  How fast can a timer input count (M4)? I want to repeat triggering an event after a certain number of counts of a very accurate clock (as fast as I can use). #advanced-timers

internal command error st-link

Posted on March 27, 2013 at 07:40When I try to debug my target board with stm32f103rbt6 with st-link (from discovery board), I get a message ''internal command error''. After, I get few messages ''Error while attempting to read 64 bytes from memory ...

ss2 by Associate II
  • 1529 Views
  • 1 replies
  • 0 kudos

Stop interrupt during BootLoader

Posted on March 27, 2013 at 02:31Hi. I am using AN2557 appilication as my base line for BootLOader. I have some question. 1. If I use the systick int during that time, is there any period I have to close it , like during FLASH programming or going t...

Barbie by Associate II
  • 1753 Views
  • 3 replies
  • 0 kudos

Flash loader demonstrator V2.6.0 command line problem

Posted on March 27, 2013 at 10:59I did not receive response for my previous question; Here is the exact description of the problem. Command below c:\''Program files\STMicroelectronics\Software\Flash Loader Demonstrator''\STMFlashLoader.exe -? return...

var2 by Associate III
  • 1448 Views
  • 2 replies
  • 0 kudos

I2C EEPROM Transmittiong and Receiving

Posted on March 21, 2013 at 11:55Hi,I am trying to send Datas to a 24C128 EEPROM via I2C interface of an STM32F4 Discovery. The problem is that I am not receiving the same value I am writing into the EEPROM. I am trying to write 0x05 into 0x00 addre...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.