2009-10-19 3:31 AM
Code execution from external RAM
#fsmc-code-execution-slow-in-sram #poorly-chosen-micro2014-01-15 11:27 AM
>> not surprising, the STM32 external bus is designed for data storage, not for code execution <<
For our application we connected the ST32F407IG via FSMC to a 8-MBit SRAM (CY7C1051DV33). We have to execute the code from the SRAM, because the code is changing during runtime. It's about 4 times slower than executed from internal flash. What is the max. speed for code execution in external SRAM (comp. to int. Flash)? If it is indeed that slow, what are the alternatives? Thanks in advance, Stephan2014-01-15 11:42 AM
It's always going to be egregiously slow. The pins transition on a 84 MHz clock, and several transitions are required for a complete transaction.
The SDRAM on the 429 is 6x slower The FLASH while intrinsically slow is protected by a caching mechanism that in some cases makes it faster than Internal SRAM. Solutions, run your code that's critical from Internal SRAM, or pick a more suitable processor with a proper cache architected into the design.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.