2009-08-04 1:15 AM
code execution from external Flash
2011-05-17 3:45 AM
Sorry for the late reply.
I just made a while(1) setting and resetting the PF6 pin. One is done in internal flash using Raisonance toolchain. One is done in external NOR flash using Keil toolchain. It s quite quicker in internal flash. I should do another test runing in external RAM. But I ll redo all test using the same toolchain. Shouldn't make a lot of difference but... I ll put the result in this post.2011-05-17 3:45 AM
Re: Test to contrast internal/external code speed execution:
Like your simple while() - suggest that you xor PF6. (monitor pin) Please try to include a variety of instructions as a ''too short'' test will magnify any loop overheads. Still have not received our EVAL-E - will perform these tests with IAR and report...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.