2020-05-10 7:44 AM
I am using stm32G031K8 nucleo board. The board was working well, it started to reset itself continuously for some time, I could only see my uart message that says started, every time I erased the code and upload previously working versions. Then it started to not execute code, now I upload led blink project but still doesnt work. I can erase the flash then upload new code.
When I try to debug it, run button is passive at the beginning.
When I press the reset button registers filled with 0xffff.
It cant go to reset handler at the beginning, how can I fix it? Thanks.
Solved! Go to Solution.
2020-05-10 8:49 AM
PC suggests running from ROM
Make sure BOOT0 pin (or options) are LOW to run user code.
If flash was previously empty you'll probably need to cycle the power.
2020-05-10 8:49 AM
PC suggests running from ROM
Make sure BOOT0 pin (or options) are LOW to run user code.
If flash was previously empty you'll probably need to cycle the power.
2020-05-10 11:00 AM
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.