2017-07-13 7:48 AM
Have been working with this guys a couple of weeks and the yare asom, but the code seems to be draining power like crasy even in stop mode 1mA.
Has any one been able to lower power consumption on stop to uA?
Solved! Go to Solution.
2017-07-20 10:05 AM
Yes Indead
st.mcu
I disabled all led configurations and initializations. And fisicaly Conected VDD_TCX0 to PA
and changed in mlm32l0xx_hw_conf.h
#define RADIO_TCXO_VCC_PORT GPIOA
#define RADIO_TCXO_VCC_PIN GPIO_PIN_10Seems that some more configuration could be missing in PA Will have to check more details when I have some time.
2017-07-13 8:07 AM
Not sat and measured. Not using in Low Power/Energy mode, but code there seems poorly executed,
bunch of grinding delay/spin loops.
This on the DISCO or your own implementation?
The DISCO has the TCXO strapped on all the time. You'd need to check the code build, that LOW_POWER_DISABLE is not defined.
2017-07-17 7:06 AM
Hi
Genskowsky.Kevin
,Based on your posts in
https://community.st.com/0D50X00009XkYNDSA3
, your problem seems to be fixed.Do you confirm? Could you please update this thread with the solution you found?
Thanks.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-07-20 10:05 AM
Yes Indead
st.mcu
I disabled all led configurations and initializations. And fisicaly Conected VDD_TCX0 to PA
and changed in mlm32l0xx_hw_conf.h
#define RADIO_TCXO_VCC_PORT GPIOA
#define RADIO_TCXO_VCC_PIN GPIO_PIN_10Seems that some more configuration could be missing in PA Will have to check more details when I have some time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.