2016-02-06 7:12 AM
I made a custom board using stm32f105rc with external 8MHz x-tal.
I think I would set the system clock with HSE,PLL,72MHz.But each stm32f105 board's SysTick_Handler timing are not same. 10,000 tick is 1 sec. In some board, 9645 tick is 1 sec, for other board, 9834 tick is 1 sec.... I think the system is not set to HSE/PLL, but HSI. But I'm not sure. Just guessing from different SysTick for all the board.My program regarding clock setting are bellow.----------stmf1xx.h#if !defined (STM32F10X_LD) && !defined (STM32F10X_LD_VL) && !defined (STM32F10X_MD) && !defined (STM32F10X_MD_VL) && !defined (STM32F10X_HD) && !defined (STM32F10X_HD_VL) && !defined (STM32F10X_XL) && !defined (STM32F10X_CL) /* #define STM32F10X_LD */ /*!< STM32F10X_LD: STM32 Low density devices */ /* #define STM32F10X_LD_VL */ /*!< STM32F10X_LD_VL: STM32 Low density Value Line devices */ //#define STM32F10X_MD /*!< STM32F10X_MD: STM32 Medium density devices */ /* #define STM32F10X_MD_VL */ /*!< STM32F10X_MD_VL: STM32 Medium density Value Line devices */#define STM32F10X_HD /*!< STM32F10X_HD: STM32 High density devices */
//#define STM32F10X_HD_VL /*!< STM32F10X_HD_VL: STM32 High density value line devices */ /* #define STM32F10X_XL */ /*!< STM32F10X_XL: STM32 XL-density devices *///#define STM32F10X_CL /*!< STM32F10X_CL: STM32 Connectivity line devices */#endifsystem_stm32f1xx.c#if defined (STM32F10X_LD_VL) || (defined STM32F10X_MD_VL) || (defined STM32F10X_HD_VL)// #define SYSCLK_FREQ_HSE HSE_VALUE// #define SYSCLK_FREQ_24MHz 24000000#else// #define SYSCLK_FREQ_HSE HSE_VALUE/* #define SYSCLK_FREQ_24MHz 24000000 */ //#define SYSCLK_FREQ_36MHz 36000000/* #define SYSCLK_FREQ_48MHz 48000000 *//* #define SYSCLK_FREQ_56MHz 56000000 */#define SYSCLK_FREQ_72MHz 72000000
#endif2016-02-06 9:04 AM
Aren't these Connectivity Line (CL) parts?
http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1031/LN1564/PF221023
2016-02-07 7:30 PM
Thank you. clive1.
I wonder why I thought 105RC was HD device...You changed your avatar.^^
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.