STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Count PWM pulses

Posted on February 08, 2016 at 10:30Hello there, I am using STM32F4. I was wondering either it is possible to count the PWM rising or falling edges that the mcu generates. I know that I could connect the PWM output to anothers timer input trigger pi...

STM32CubeMx problem creating MDK-ARM V4 Project

Posted on January 30, 2016 at 22:18I have found a problem with the latest version of STM32CubeMX 4.12.0. Each time I generate the sources with an MDK-ARM V4 project it duplicates the source files in the .uvproject file. The attached picture shows th...

Timer issue

Posted on February 08, 2016 at 17:03Hi,I'm having an issue setting up TIM1 for PWM on the STM32F446.In the following code, the PWM works for TIM2 but not for TIM1.Any ideas?Thank you.  RCC->APB1ENR |= (1UL << 0); // TIM2 clock enable  TIM2->PSC   = ...

kalhana by Associate II
  • 1990 Views
  • 4 replies
  • 0 kudos

Fluent frequency modulation

Posted on February 08, 2016 at 09:59 Hello there, I am using STM32F4. I am trying to make an application, where I could be able to modulate the frequency (not pwm) of one channel for example in range of 1k - 20k Hz. The problem i encountered...

Question regarding Bit-Banding

Posted on February 08, 2016 at 09:02Hello. I try to use bit-banding feature in a STM32F303 uC on GPIO registers (exactly to change mode of a pin in MODER register). But as I see, all GPIO registers in that uC are on addresses which starts with 0x48....

matic by Associate III
  • 1091 Views
  • 3 replies
  • 0 kudos

problem with interrupts (stm32f103re)

Posted on February 07, 2016 at 09:54Hi I configured 2 EXTI (PA0 & PB1 ) and work perfectly. But when I configure Port B pins output and connect a led to them ( or even a wire!) inerrupts occure! (I pulled up intrnally and externally PA0 & PB1 and in...

Clock setting for stm32f105rc

Posted on February 06, 2016 at 16:12I made a custom board using stm32f105rc with external 8MHz x-tal.I think I would set the system clock with HSE,PLL,72MHz.But each stm32f105 board's SysTick_Handler timing are not same. 10,000 tick is 1 sec. In som...

paul0208 by Associate III
  • 1373 Views
  • 2 replies
  • 0 kudos

ASM error when using an array containing struct elements

Posted on February 07, 2016 at 19:55 Hello, I have an array, that should contain structures for the input and output pins as follows: typedef struct inputStruct { uint16_t pin; GPIO_TypeDef *port; }input_t; struct inputStruct inpu...

sven23 by Associate II
  • 3270 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.