2024-04-12 4:05 AM
Hello
I have watched the lab about stm32wb55 where the board receives any event from the smartphone app and toggles the onboard LD2.
Now i want to make mine specific by checking for the received value and only toggle the LD2 if its a 1 and only turn it off if its a 0.
i have tried using the code below but it is not working well can someone assist me
attribute_modified = (aci_gatt_attribute_modified_event_rp0*)blecore_evt->data;
if (attribute_modified->Attr_Handle == (CustomContext.CustomMycharwriteHdle + CHARACTERISTIC_VALUE_ATTRIBUTE_OFFSET))
{
return_value = SVCCTL_EvtAckFlowEnable;
/* USER CODE BEGIN CUSTOM_STM_Service_1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
uint8_t* receivedData = attribute_modified->Attr_Data;
// Check the received value and perform actions based on it
if(receivedData[0] == 1) {
// If the received data is 1, toggle the LED
HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin);
} else if(receivedData[0] == 0) {
// If the received data is 0, turn off the LED
HAL_GPIO_WritePin(LD1_GPIO_Port, LD1_Pin, GPIO_PIN_RESET);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.