2022-05-25 7:49 AM
HI,
I want to change tim1 Dead-time generator setup continuously between 10 -120
first time I set Dead-time with cube mx and it worked correctly
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 10;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}then i wrote a function to change that with variable
void user_deadtime(uint8_t value)
{
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = value;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
}it didnt work , after first change ,pwm will be stop
i try to that with registers
void user_deadtime(uint8_t value)
{
uint32_t temp;
temp=TIM1->BDTR;
TIM1->BDTR=temp|value;
}and i got same result . after first change , pwm will be stop
i debug it and i understood that when i set TIM1->BDTR the value will not change , and it got wrong value that i never set that.
how can i set that after continuously ?
i am using stm32f746
thanks
2022-05-25 2:27 PM
> i debug it and i understood that when i set TIM1->BDTR the value will not change
Why do you think so?
> and it got wrong value that i never set that.
What value?
What is content of BDTR before and after calling given function? Is BDTR.MOE set? What is content of other TIM registers when PWM stops to work?
JW
2022-05-25 5:30 PM
TIM1->BDTR=temp|value;It doesn't do what you think it does. This is why a basic programming must be learned first...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.