2012-12-11 4:05 AM
Hello all experts,
I have configured the TIM2 timer of my stm32f4 discovery board. Now I want to change the prescalar value of it on the go. My code is as follows ************************************************** void TIM2_IRQHandler(void) { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) { TIM_ClearITPendingBit(TIM2, TIM_IT_Update); GPIO_ToggleBits(GPIOA, GPIO_Pin_5); } } ************************************************* void INTTIM_Config(uint16_t numOfMilleseconds) { NVIC_InitTypeDef NVIC_InitStructure; /* Enable the TIM2 gloabal Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = (500*numOfMilleseconds) - 1; // 1 MHz down to 1 KHz (1 ms) //TIM_TimeBaseStructure.TIM_Prescaler = 84 - 1; // 24 MHz Clock down to 1 MHz (adjust per your clock) TIM_TimeBaseStructure.TIM_Prescaler = 168-1; //168MHz Clock should be down to 1MHz TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); /* TIM IT enable */ TIM_ClearITPendingBit(TIM2, TIM_IT_Update); TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); /* TIM2 enable counter */ TIM_Cmd(TIM2, ENABLE); } *********************************************** int main(void) { GPIO_config(); INTTIM_Config(50); while (1) { } } **************************************************** Initially I configure the timer to give an interrupt in 50ms duration and it succeeds. Now I want to change the interrupt duration to 100ms when I receive my first interrupt. I tried to adding this to the irq TIM_TimeBaseStructure.TIM_Period = (500*40) - 1; // 1 MHz down to 1 KHz (1 ms) TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); But I couldn't get the required output. Please advice me on how to achieve this task. I know this can be done since the datasheet states the preamble can be changed on the go. Thank you for your valuable time. Thilina #dividers-and-prescaler-division2012-12-11 4:36 AM
For the PERIOD
TIM2->ARR = NewPeriod; // n-1 For the PRESCALER TIM2->PSC = NewPrescaler; // n-1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.