STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F0discovery PWM with external clock and trigger

Posted on November 13, 2012 at 17:38 I want to create a simple PWM implementation which uses an external clock source and is synchronised to a trigger pulse (one pulse per PWM period). I need at least three (ideally four) channels of output with...

Software reset in STM32Discovery

Posted on December 01, 2012 at 22:27I need to configure a software reset so that it occurs when my firmware detects that my ADC value has reached a maximum or a minimum value. I realise that I need to have a RCC interrupt.Is there someone who can he...

terence-b by Associate II
  • 1526 Views
  • 3 replies
  • 0 kudos

Stm32f407 Discovery IAP pgm

Posted on December 11, 2012 at 15:49How to use the hex2bin.exe? i have hex2bin.exe.1.I want to convert the user program hex file to user program binary file.another one is2.how to change the load address of the user program.i am using the keil compi...

vinothraj by Associate II
  • 1502 Views
  • 2 replies
  • 0 kudos

STM32L unstable at high frequencies

Posted on December 11, 2012 at 02:23 My STM32L151RCT seems to become unstable when I set the SYSCLK to PLL=26MHZ. Lower frequencies (say, 20MHZ) appear to be solid. The failure mode is inconstantly a HardFault, or stack pointer gets ...

Change TIM2 prescalar value on the go

Posted on December 11, 2012 at 13:05Hello all experts, I have configured the TIM2 timer of my stm32f4 discovery board. Now I want to change the prescalar value of it on the go. My code is as follows **************************************************...

tybandara by Associate II
  • 1115 Views
  • 1 replies
  • 0 kudos

Nichelite - Doesn't include FIN packet support?

Posted on December 11, 2012 at 12:32I've been using Nichelite on a STM32F107 and have come to the conclusion that it doesn't fully support the TCP/IP protocol in that it doesn't produce FIN packets when a connection is closed. Can anybody confirm th...

TIM2 Interrupt issue

Posted on December 11, 2012 at 09:30Hello all experts, I configured the TIM2 in my STM32F4 discovery board such that it gives me interrupts every 50ms. The code is as follows. ********************************* void TIM2_IRQHandler(void) {   if (TIM_...

tybandara by Associate II
  • 1485 Views
  • 1 replies
  • 0 kudos

STM32f217IG SPI Master MISO question

Posted on June 07, 2012 at 08:55I have read through many posts about SPI problems and configuration questions.  I feel I have everything configured correctly, however I do not receive any data transferred across the MISO line.  Below shows the confi...

rmpresto by Associate II
  • 3346 Views
  • 9 replies
  • 0 kudos

I2C problem

Posted on December 03, 2012 at 10:23I am a beginner about the microcontoroller. I use STBee. I want to connect a STBee and a sensor(IMU 6DOF ITG3200/ADXL345). At first I want to let you display a value of the x-axis. Please teach a solution. &sharpi...

s1170198 by Associate II
  • 3136 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.