2023-05-12 3:51 AM
I want to change system clock as a PLL(using HSE) 20 Minute after systemInit. thats why I must change it in main function not system_stm32f0.c file.
Here is my code, Not working properly. I dint do anything interrupt function.
void ClockInit(void)
{
if ((RCC->CFGR & RCC_CFGR_SWS) == RCC_CFGR_SWS_PLL)
{
RCC->CFGR &= (uint32_t) (~RCC_CFGR_SW);
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_HSI) {}
}
RCC->CR &= (uint32_t)(~RCC_CR_PLLON);
while((RCC->CR & RCC_CR_PLLRDY) != 0) {}
RCC->CFGR &= ~(RCC_CFGR_PLLMULL | RCC_CFGR_PLLSRC);
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_Div2 | RCC_CFGR_PLLMUL5);
//RCC_PLLConfig(RCC_CFGR_PLLSRC_HSI_Div2,RCC_CFGR_PLLMUL5);
RCC->CR |= RCC_CR_PLLON; /* (7) */
while((RCC->CR & RCC_CR_PLLRDY) == 0) {}
RCC->CFGR |= (uint32_t) (RCC_CFGR_SW_PLL);
while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL) {}
SystemCoreClockUpdate();
}
Thanks for everything
2023-05-12 4:51 AM
What are exactly the symptoms?
Code looks good. Can't you single-step and observe the registers?
Which STM32? The 'F0 family has two different RCC setup (PLL prescaler).
JW
2023-05-13 12:01 AM
Did you adjusted the FLASH latency and APB prescalers properly before increasing the SYSCLK?
2023-05-15 3:26 AM
STM32F030C8T6TR
I changed code like that, it seems good
void RCC_HSE_Configuration(void){
RCC_DeInit();
RCC_HSEConfig(RCC_HSE_ON);
if(RCC_WaitForHSEStartUp() == SUCCESS){
RCC_HCLKConfig(RCC_SYSCLK_Div1);
RCC_PLLConfig(RCC_PLLSource_PREDIV1, RCC_PLLMul_4);
RCC_PLLCmd(ENABLE);
while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
while(RCC_GetSYSCLKSource() != 0x08);
}
SystemCoreClockUpdate();
}
2023-05-15 3:28 AM
No, I don't quite understand, can you show an example code?
2023-05-23 4:30 PM
Reference manual has an explanation and even exact sequences of actions listed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.