2018-02-12 5:26 AM
hello
i use this configuration for send for ws2812.
GPIO_InitStructure.GPIO_Pin = WS2812B_PINS;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;GPIO_Init(WS2812B_PORT, &GPIO_InitStructure);
I because i need 5v i use this configuration (use 2.2K for pull up). but i now i want chage port to pp and 3.3 v and do this configuration
GPIO_InitStructure.GPIO_Pin = WS2812B_PINS;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;GPIO_Init(WS2812B_PORT, &GPIO_InitStructure);
but i have a problem if the mcu use to open drain if i change to pp i have noise on it but if it is new i don't have any problem what can i do?
2018-02-12 5:42 AM
are you discussing the serial LED driver ?
its likely to work with 3V data in,. did you try it ?
you can use a transistor or FET to translate the voltage, but some configurations invert the data, some don't.
easiest is: 2 resistors, 1 npn transistor but returns an inverted output.
2018-02-12 5:55 AM
but i have a problem if the mcu use to open drain if i change to pp i have noise on it but if it is new i don't have any problem what can i do?
If I understand this convoluted and careless punctuated sentence correctly: Have you tried a proper de-init of the pin ?
Un-set the old pin configuration first, then set the new one.
... if i change to pp i have noise on it...
This suggests you did not really change to PP, I view 'noise' as symptom of OD without a load resistor.
2018-02-12 6:37 AM
if i change to pp i have noise on it
on what, exactly?
And what sort of 'noise', exactly, is it?
Post a proper schematic of your two setups, and oscilloscope traces of the signals.
Instead of changing to PP, what happens if you just set PP from the outset ... ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.